Customer is having issues with TPS536015 going into hiccup mode on 10% of their board assemblies and not recovering. The TPS536015 is used to generate a 5V supply that powers downstream regulators generating 3.3V, 2.5V and 1.2V.
Reducing the output capacitance on the downstream regulators resolves the issue.
What is the best way to work around this issue on the TPS536015 without reducing the output capacitance?
Could we use TPS536015 !RESET to drive the enable pins of the downstream Vregs to reduce startup current?
What about using an RC on the TPS536015 EN pin to extend startup time?
Please advise.
Thanks,
Mark