Other Parts Discussed in Thread: BQSTUDIO, BQ34Z100
I have been successfully using the BQ34Z100EVM for several weeks now, and was able to transfer between sealed, unsealed and full access modes. However, recently I have found that the device refuses to transition away from an unsealed state. Strangely, after a power cycle or reset the chip defaults to a sealed state, as expected, and I am able to transition to an unsealed state with no problem, indicating that the access keys for this are correct. However, when I try to return to a sealed state using the control sub-command 0020h, it refuses to do so.
I am also unable to transition to full access mode, although I am sure that the default key (FFFFFFFFh) has not been changed. I have tested this with both my own microcontroller code and with the Battery Management Studio with the same results. All other device functions are functional, such as reading/writing flash locations.
Does anyone have any idea why this is happening?