Other Parts Discussed in Thread: TPS2540, TPS2546
Hello,
I am currently designing a board to have the capability of charging a Samsung Tablet about 100% of the time. I checked your eval board USB connector and it looks like it is rated at 1 Amp, however your board data sheet details a max of 2800 mA (2.8A) of current for downstream charging. Is there something I am missing or is the current going to be limited to 1A for charging? It seems like the connector shouldn't be able to hand more than 1A max. Also is the TPS2540 tested with Samsung tablets? If I plan to use Ipad or Samsung Tablets is the TPS2540 part interchangable with either tablet?
Thanks,
Mike