Hi,
I have few queries on Controlling Charging and Discharging and Monitoring the Super Caps(24V).
Application: Input will be 24V,20A from the power supply and when in power outage it should power(24V,3A) the controller for 3 seconds.
Are there any reference example for this application?.
I found BQ24640 but as i noticed this IC is charger which is like Buck If input is 24V then Super capacitor must rated slightly lesser the voltage of input. Is my understanding correct? But in my case Supercaps has to charge up-to 24V.