This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65218D0: PMIC Enable Issue. Continously tries to turn out but disables immediately.

Part Number: TPS65218D0

Hi there,

The TPS65218D0 we are using on our design continuously tries to turn on but immediately disables. We want to set it so it turns on as soon as power is applied and not rely on the push button input. What have we wired wrong? See attached for a snapshot of the schematic.

  • Hi Tony,

    This schematic indicates that the switch nodes of the DCDC1, DCDC2, and DCDC3 are incorrectly connected directly to the output capacitors, bypassing the inductors.

    The inductors should instead be placed directly between L1, L2, and L3 and the output capacitors, with FB1, FB2, and FB3 directly connect to the output capacitors.

    To boot automatically and remain active whenever power is applied, PWR_EN may be pulled up to +5V instead of the 1.8V rail.

    Best Regards,

    Rick S.

  • The inductors being in the wrong place should not prevent the unit from staying powered up. And with the PWR_EN pulled to +5V the PMIC still does not stay on. 

  • Hi Nick,

    Please monitor FB1, FB2, FB3, and PGOOD with an oscilloscope during the restart behavior.

    The datasheet indicates that power good faults will cause the device to reset. The pgood thresholds are observed using the FB nodes of each regulator.

    Best Regards,

    Rick S.

  • Nick,

    Is R97 installed? It does not say "DNP" (but other resistors, like R16, specifically say "DNP").

    If R97 is installed, then you should remove it.

  • Nick,

    I also agree with Rick that the incorrect placement of inductors L1, Le, and L3 will have very negative effects on the performance of the system. This wiring will not work and will result in frequent resets. Every time the high-side FET is closed, the output voltage will ramp up to the input supply very quickly (the only thing slowing it down is the output capacitor), resulting in an overvoltage (VOVP) fault. Then the low-side FET is closed and the output voltage will sharply drop to 0V, resulting in an undervoltage (VPG) fault. This will never result in a stable output within regulation.

  • Yes, we rewired the inductors to put them in the correct spot and the DC-DC's came up :) Thanks for the assistance. We did not fully understand the internals of this component when we did the design.