Other Parts Discussed in Thread: TPS25942A
Hi,
I'm designing a circuit which has following specification.
Input Voltage 5 - 6.2 V
Input Current 5A
Output Voltage 5V
Output Voltage 5A
According to the TPS2400 datasheet, above specifications can be satisfied by using TPS2400 IC.
My question is how can I simulate TPS2400 based circuit? (currently I'm using NI Multisim)
Is there another simulation software that I can use for simulate TPS2400 based circuit or can someone give me a TPS2400 NI simulation component?