Other Parts Discussed in Thread: BQSTUDIO, GPCCHEM, GPCRA0,
Hello team, I submitted log files, but doesn't receive any reply from gpc or ChemID team.
Any suggestions?
you can find the log file here.
Thanks in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello team, I submitted log files, but doesn't receive any reply from gpc or ChemID team.
Any suggestions?
you can find the log file here.
Thanks in advance.
Here is your report. You need to log again at a 1s interval and relax the cell for 5 hours.
Adjusted Log interval in Preferences as 1000ms,. the BQstudio is not generating as accurate 1s interval.
I attached the log file here, please check and letme know.
Thank you
Thu Jun 27 10:09:06 CEST 2019 Device Name = bq34z100G1 Firmware Version = 0_16 Sample,DateTime,ElapsedTime,Control,CtrlStatus,StateofCharge,MaxError,RemCap,FullChgCap,Voltage,Current,AvgCurrent,Temperature,AverageTimeToEmpty,AverageTimeToFull,AvailableEnergy,AveragePower,InternalTemperature,CycleCnt,StateofHealth,ChargeVoltage,ChargeCurrent,PackConfig,Flags,Flags B,GridNumber,LearnedStatus,DoDatEOC,Qstart,TrueRC,TrueFCC,StateTime,DOD0PassedQ,DOD0Time,DOD0,QmaxDOD0,QmaxPassedQ,QmaxTime,LogRowTime(ms),LogStatus 1,2019-06-27 10:09:07,1.009,0x0000,0x0014,0,100,0,0,11160,0,0,26.1,65535,65535,0,0,28.6,1,0,15500,376,0x49D9,0x0116,0x2400,0,0,16384,0,-300,0,4045,0,17,16384,0,0,17,1133,SUCCESS 2,2019-06-27 10:09:08,2.212,0x0000,0x0014,0,100,0,0,11160,0,0,26.1,65535,65535,0,0,28.6,1,0,15500,376,0x49D9,0x0116,0x2400,0,0,16384,0,-300,0,4046,0,17,16384,0,0,17,1091,SUCCESS 3,2019-06-27 10:09:11,4.756,0x0000,0x0014,0,100,0,0,11160,0,0,26.1,65535,65535,0,0,28.6,1,0,15500,376,0x49D9,0x0116,0x2400,0,0,16384,0,-300,0,4049,0,18,16384,0,0,18,1134,SUCCESS 4,2019-06-27 10:09:12,5.946,0x0000,0x0014,0,100,0,0,11160,0,0,26.1,65535,65535,0,0,28.6,1,0,15500,376,0x49D9,0x0116,0x2400,0,0,16384,0,-300,0,4050,0,18,16384,0,0,18,1443,SUCCESS 5,2019-06-27 10:09:15,8.842,0x0000,0x0014,0,100,0,0,11160,0,0,26.1,65535,65535,0,0,28.6,1,0,15500,376,0x49D9,0x0116,0x2400,0,0,16384,0,-300,0,4053,0,18,16384,0,0,18,1055,SUCCESS
here is the log file attached with 1s interval and relax cell for 5 hours, looking forward to receive the ChemID.
Thanks in advanceBK220SCHU_1_ChemID.zip
Hello team,
I'm writing on behalf of my customer;
Issue regarding ChemID, it’s not resolving from days.
hereby I've attached two files, one received from gpc calculator and the log file obtained from the BQStudio.
The log file is in this order
Relax 2hrs
Charge to- charge termination
Relax 5hrs
Discharge to- current 0A
Relax 2hrs
The report says First OCVpoint has non-zero current I= -0.008 Please make sure you have a 2 hr relaxation period before the beginning of discharge, but I didn’t see I=-0.008 A.
Any suggestions?
Thank you and best regards,
Adrian4024.GPC_report.zip
Hi Adrian,
Looking into the log there are severe discontinuities in the data. You need to follow the instructions in the GPCCHEM page completely. We need a log with a short relaxation at the start from a fully charged cell and a dsg to empty and short relaxation after.
Your elapsed time also has to be in seconds. Please follow all the instructions here, and then upload the data to the tool.
Hi Batt,
on behalf:
Fuel gauge BQ34Z100-G1 the GPCRA0 cycle is performed, report email received from gpc_do_not_reply@ti.com, but unfortunately its empty. The report and error email image is attached for reference.
Looking forward for feedback or support.
BR,
Adrian
Hi Adrian,
Why do you need GPCRA optimization? A normal chem ID has a wider range when left at defaults. You have a chem ID already, you don't need to do further optimization unless you are getting really bad accuracy with it.
Hi Batt,
Chem ID is obtained, as we discussed earlier in this link where the Ra values for a lower cap cell will be different from the other cell that it matched. The GPRCA is performed to verify the Ra and Qmax tables, but unfortunately we didn't receive report.
Thanks
Hi Reddy,
To get the correct Ra values for your battery after you found out the chem ID, you should run a learning cycle. Now a GPCRa cycle helps with Ra0 optimization incl thermal parameters, however, your learning cycle is necessary before this is performed. This will optimize your learned values for a room temp run.
Please run a learning cycle first so that your Ra values can be determined.
Hi Reddy,
The screenshot shows that the battery has not learned. If you did learn resistance, it will have updated the Ra flags in the first cycle to 0x0055 and in the second cycle to 0x0000 and 0x0055. Please make sure your battery is relaxed with RDIS reset before starting your charge and dsg cycle when you run your learning cycle.