I’m trying to design a dual-output flyback circuit using the LM2587T-ADJ chip. Input would be 30 volts while outputs would be +/- 15 volts and each drawing 3 amps each. Figure 26 of the LM2587 datasheet seems to be a good starting point. Resistor and potentiometer will have to the added from FB (pin 2) to the (+) Vout side of the transformer secondary. Also, components to be used have to be sized up for the correct power requirement.
My question is, could I really use the circuit in Figure 26 and attain the outputs that I needed or am I completely off. If I am off, could you provide guidance?
Also, I am unsure as to how to accurately calculate the input power requirement of my circuit. When trying to calculate the input current requirement this is how I estimated it (assume efficiency is 70%):
(input power) * efficiency = output power
(30 volts * X amps) * 0.7 = 30 volts * 6 amps
X amps = (30 * 6) / (30 * 0.7) = 8.57 amps
Is the calculation correct? If it is, another question is, would the 8.57 amps be the switched current?