Part Number: TPS65218D0
Other Parts Discussed in Thread: TPS65218, , BOOSTXL-TPS65218
Hi
This is waveform is power down of AM737xEVM.
Yellow:Input, Green: 1.8V, Blue: 3.3V
1.8V and 3.3V are power down at the same time.
AM437x datasheet 5.12.1.3 is written as follows;
"If it is desired to ramp down VDDS, VDDS_CLKOUT and VDDSHVx [x=1-11] simultaneously, it should always be ensured that the difference between VDDS, VDDS_CLKOUT and VDDSHVx [x=1-11] during the entire power-down sequence is <2 V. Any violation of this could cause reliability risks for the device."
However, I think that there is not the circuit guaranteeing this issue in TPS65218 or external circuit.
The installation device of EVM is TPS65218B1, will the falling timing be improved in D0?
Please teach me how we should do this circuitry.
Best Regards,
PAN-M