Hi Team,
I have three questions about TPS717. Could you answer following questions?
1. Let me confirm if the Ifb value is typo or not.
The I_FB max is 1uA so it might introduce 0.32V offset by 320kohm FB divider…
2. Is it possible to use 10k to 100k resisters as FB voltage divider?
Although i'm understanding the datasheet recommends to use 160k~320k register as R2, my customer want to use smaller value due to the leakage discussing above.
3. What frequency range should be met for ESR requirement for stable operation? Also are there any min ESR requirements for stable operation?
Datasheet requests to chose less than 1 ohm ESR cap for stability reason but ESR of cap fundamentally has variations depending on frequency.
At low frequency range, almost cap tends to have 1 ohm or larger ESR.
Regards,
Takashi Onawa