Part Number: TPS65720
Hi!
I want to reduce the charge current in a product I am developing when the temperature is below a certain degree.
From what I can see in the datasheet for the TPS657201 PMIC the TS_OUT pin can be used to read a voltage that corresponds to a temperature. The voltage interval is 0 to 1.4V and the corresponding temperature scale is -20 to 60 degrees Celsius. How is this conversion made? Is it a linear conversion?
How would one go about to get a battery temperature measurement using the value from the TS_OUT pin?
Thanks in advance!
Best regards,
Björn