Other Parts Discussed in Thread: BQ28Z610,
Hello,
I have download the v 1.3.93 from web site but the installation file is 1.3.90 Build 1 and the date of release from the web page and the installation package are different.
Anyway, I have installed in a clean directory and at first run everything seemed good but later I have been facing some troubles:
1) it seems that starting with EV2300 connected to the board, the SW doesn't recognize the type of BQ attached (in this case BQ28Z610)
2) even on my PC, sometimes the link between EV2300 and bqStudio has some difficult to estabilish
3) the AdvComm is not working well: many times the write/read memory or registers operation gives different results: writing 35 00 to 3e register, the reading is 56 00 etc... I has not been able to change the sealing keys.
Using the previous 1.3.86 version, all those issues are not present and I change the unsealing keys at the 1st attempt. I have re-installed the 1.3.86 .... and I wait for a further version.
Hope this will be useful
Maurizio