Part Number: UCD3138PFCEVM-026
Hi engineers:
About UCD3138PFCEVM-026 Programm
I download the code(PWR026_PFC) from TI website, and debug by CSC, but I need help for some promblems. Even if I change the CCS edition , the problem is not solved. See the problem:
warning #10366-D: automatic library build: using library "E:\win
10\ccs9.1.0\ccs\tools\compiler\ti-cgt-arm_5.2.5\lib\rtsv4_T_be_tiarm9.lib"
for the first time, so it must be built. This may take a few minutes.
'e:/win' It's not an internal or external command, nor a runnable program, Or batch files.
>> ERROR: mklib: gmake error during rtsv4_T_be_tiarm9.lib build
warning #10207-D: automatic RTS selection: resolving index library "libc.a" to
"rtsv4_T_be_tiarm9.lib", but "rtsv4_T_be_tiarm9.lib" was not found
error #10010: errors encountered during linking; "PWR026_PFC_UCD3138064.out"
not built
>> Compilation failure
makefile:175: recipe for target 'PWR026_PFC_UCD3138064.out' failed
gmake[1]: *** [PWR026_PFC_UCD3138064.out] Error 1
gmake[1]: Target 'main-build' not remade because of errors.
makefile:167: recipe for target 'all' failed
gmake: *** [all] Error 2