Hi,
I am using TPS40422 device in two-phase single 3.3V output mode and we are trying to read current values at READ_IOUT register 8Ch for total current consumed on this power rail.
Do we need to add the measured current at 8CH by selecting channel 1 and channel 2 using the PAGE register 00h for a total current?
or Since the device operates two-phase mode it is not required to add channel 1 and channel 2 current?
PAGE select register value does not matter for READ_OUT in the case to two-phase mode?
Thanks
Sivaguru