In the situation of concern, the power good pin is pulled-up to 3.3V through 20kohms and there is a 0.1uF capacitor connected to ground.
The abs max current for the PG pin is 10mA. Is there any chance of damage to the LMZ30606 device if the PG pin goes low and discharges the 0.1uF capacitor?
What value of capacitance would cause a problem considering that 1/2 CV^2 would be dissipated int he internal pull-down FET?