Hi,
Currently we thought of using the TPS7A19 in our design with input voltage in the range of 11 to 28volts with 3.3V output. Our load requirement will be in the range of 150 to 200mA. Will I be able to use this part for this requirement.
Problem we are facing with this device is output voltage is dropping to 2.45V when my load requirement is 100mA (when the load is 22ohm). Only when my load is less than 10mA then only the device is working fine. Can you please help us in solving this issue.
Thanks,