Other Parts Discussed in Thread: BQ34Z100, BQ34110
I am trying to run a chem ID on a primary LiSO2 battery (BA 5590 B/U).
This type has a max OCV of 15V, consisting of 5 cells (3V each).
Capacity is 15Ah.
Termination voltage is 10V (2V per cell).
I ran the discharge test at C/10 as required and the results are attached. I have also attached the ID test submission zip file.
However, I am only getting a very inaccurate match:
"Best chemical ID : 700 Best chemical ID max. deviation, % : 99.5
Accuracy Error: Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recommended format, units and test schedule"
There is no anomaly in the date that I can see, but this chemical ID is definitely not the correct one as it pertains to a Lithium Titanate rechargeable battery type. I have not been able to find a LiSO2 battery type on the ID list, so am wondering if I am going to be able to ID this battery at all?
If not, what does 99.5% max deviation actually mean? How will it affect the gauging accuracy if I use it as my ID? I.e. what will my max error be on my state of charge measurement? Will I even be able to run a learning cycle?