Hi Support team
I am working on a customer application for an industrial camera. The issue I am having is the tps92602 is not responding fast enough to the frame clock and also to changes in the load conditions.
In the LED bank, one bank contains 8 leds in 4 sets (2 leds each set). THhy are using discrete fets to change the number of LEDS in the string for shadowing. The issue we are having is when we try to pulse at 120 frames per sec, the device is not responding fast enough. We are driving a string of 8 LEDS 4.2v each at 1.5~2 Amps. They may drive all 8 LEDS at once or just 2 LEDS via the switching network.
My two questions are is the the best part, I am using a dual because there are two different LED Banks? Second, is there a way I can speed up the response on the evm? They are testing boost to battery, they have a 12 volt input.
Thanks
Jeff Coletti