Hi Experts,
Could you give us some suggestions for how to eliminate the high frequency jitter during ramp up ,thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Youhao,
Please see the sch file as follows,Vin : 5V , Vout : 12V, No load,thanks., the design has capability for 10A load.
After that , we are following the all parameters of EVM board except inductor(now 17u H) to see whether it has same behavior,yes it was.
The Vin 5V drop was dropping during ramp up ,we have checked the
Hi Han,
The schematic basically looks okay. However, the current sense of 2mOhm appears to be too small. I also noticed the inductor current peaks up to 20A in the above waveform. Since Vin is supplied by your input source, it seems the 20A exceeds the source's current limit and it collapses. Can you double check your input source current limit?
Thanks,
Youhao
Hi Han,
A very large output capacitor will defeat the internal soft-start function. The soft-start basically achieves two things by limiting the duty cycle: reducing the inrush current and also the output voltage overshoot. Your large capacitor is not fully charged up after the internal soft-start is completed, and a large current is still needed, with max duty, to charge the capacitor, and the input current can exceed your source and bring the voltage down.
Thanks,
Youhao