Dear,
When testing the LM5141-Q1EVM, i find some questions.
1.In light or very low load conditions, with the increase of Vin, the Iin decreases to 0 which i think enters standby mode. And, in this condition, i can see pulse in Iin, the frequency is around 2.5kHz and the amplitude is lower when Vin increases, which is 264mA when Vin=12V. What's the problem?
2.In light or very low load conditions, Pin decreases with the increase of Vin; while when the load increases, Pin increases with the increase of Vin, So, what causes the difference?
3. with the increase of load, when Vin is just a little higher than 5.5V, the output is not 5V instead of 4.8V or lower. What's the problem? I used to guess the dutymanx of 5141, but the Vout/Vin is higher than 80%. Is my measurement wrong?
4.When i change the load, why does Vin react with a ripple, and the ripple amplitude is proportional to Vin?
Regards
Wenyi