Other Parts Discussed in Thread: BQ25895, BQ2980
In my application, I have to use 2x 18650 batteries in parallel for capacity reasons. At the same time, for marketing reasons, I need to use removable 18650 elements, using a battery holder on board, and so the chance that batteries might be inserted backwards is definitely not negligible.
I was thinking of protecting each battery with a BQ2970, adding an extra mosfet to keep the charge mosfet off, as mentioned in a few posts, and then connect the output of the two protection circuits in parallel.
Would this work? or would you recommend a better/alternative solution?
FYI the charger is implemented using a BQ25895 on the main board - and hence can never be connected wrongly.
Looking forward to reading from you.
Gabriele