HI,
Is the body diode Schottky in the CSD17308Q3?
I can hardly find an answer in the datasheet.
Thanks,
Joshua Kim
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI,
Is the body diode Schottky in the CSD17308Q3?
I can hardly find an answer in the datasheet.
Thanks,
Joshua Kim
Joshua,
Thanks for considering our MOSFETs.
The CSD17308Q3 does not have a schottky diode it is the standard body drain diode all MOSFETs have.
If a MOSFET does have a schottky diode, as this take additional processing, manufacturers normally highlight this on the front page of the datasheet as this is not the standard. TI does not offer MOSFETs with integrated schottky diode,
Another way to quickly check if a part has a schottky diode integrated or not is to look at the Vsd of the device. If around 0.5V, then this is likely a schottky diode, if around 0.8-1V then the std mosfet junction diode. Also FETs with schottky diodes have much higher Idss leakage, they will typically have leakage specs in the 0.5mA max vs std FET 1uA , so 500x larger.
I hope this helps
Dear Chris Bull,
Thanks for the answer, which clarified my question altogether.
Thanks again,
Joshua Kim