Team,
We are using LM5030 and have some issues with spikes on CS (R123) resistor.
Those spikes are 2V and CS pin is activated at every period and is triggering overcurrent protection of IC so the output is “choked”.
Below you can see captured waveform of PCB:
|
Waveform |
Component |
|
Ch2 |
R123 |
|
Ch3 |
Drain of Q2B |
|
Ch4 |
Drain of Q2A |
Those spikes are made by switching of Q2B (schematic attached here: push_pull_converter.pdf).
Outputs are loaded with:
|
Output |
Load |
|
+DC_HS |
31.4R |
|
-DC_HS |
11R |
|
+DC_LS |
31.4R |
|
-DC_LS |
11R |
The maximum VDS of FETs is 100V (http://www.vishay.com/docs/75213/sqjb70ep.pdf)
The VIN is 30V.
- Do you have any advice to help us with this problem?