Other Parts Discussed in Thread: UCC24612,
Hello,
I am using the UCC24612-1DBVR in a POE supply. This power supply, a TI-design (TIDU190-January 2014), has a 12V 15W fly-back topology.
In the DCM mode (Discontinuous Conduction Mode) everything works fine.
When the power supply has to provide more than approx. 10W, the converter enters CCM (Continuous Conduction Mode).
In the CCM the PowerFET is switched off too late, which introduces a momentary short that leads to a very strong spike.
All this leads to the PowerFET and snubber resistor becoming very hot.
Leaving out the snubber doesn't change behaviour of UCC24612, PowerFET still becomes very hot when converter enters CCM.
The PowerFET type is FDMC102L, VDD and REG voltages are stable and the gate has a 2 ohm resistor as recommended in the data sheet.
Is there something I forgot?
Best regards,
Chris