Part Number: ISO5452
Other Parts Discussed in Thread: ISO5852S
Hi team,
My customer was using ACPL-337J for HVAC compressor projects and I think I've identified their current design challenge and would like to see if ISO5452 can solve it.
Description:,
Customer was using ACPL-337J to drive FF600R12IP4. The system OCP is set to be 1200A, desaturation current is set 2400A. The target is to keep VCE<1200V whenever short happens. ACPL-337J can only initiate soft turn-off after hitting desaturation current(2400A), which means the VCE may be above 1200V during current rising from 1200A to 2400A. In order to solve the problem, customer is using a big RES for shut-down. The efficiency get worse as a compromise.
I notice that ISO5452 can initiate soft turn-off right after OCP(1200A), then enter Desat(2400A). It might help solve the problem.
Can you double check with my assumption above? And if your team can provide more details or test data, it would be very helpful for me to engage customer.
Thank you and looking forward to your reply..
Regards,
Patrick