I would like to use the BQ2970 battery protector to act like a low battery indicator. I am using a voltage regulator which can be put into sleep mode (when a pin is pulled logic LOW - the over discharge mosfet pin would control my regulator perfectly) using a protection IC. I would like to use another device which better suits my application or how I can use this device. The problem I am having is that on the V- pin there will be unexpected behaviour as no MOSFETs are present. Thank you for any help.