This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61096A: can the three pins(FB,EN ,VIN )connect togethe to get fixed 12 V output?Vin=5V

Part Number: TPS61096A
Other Parts Discussed in Thread: TLV61046A

Hello~

Vin is 5V,and I need TPS61096A boost to 12V or 13V for PMOLED panel driving power supply.

1.To  simply achieve 12V output,the three pins FB,EN,VIN are connected toghter. Is it OK or not? I don't need to control TPS61096A enable or disable.

2.If VIN=5V  and VOUT=13V,can you help to calculate the value of external resistor divider R1 and R2(FB pin)?

Thanks