Hi Team,
My customer is asking a question regarding TPS7A84.
In 6.1 Absolute maximum ratings, SNS,OUT's MAX is VIN+0.3V or 7V, whichever is smaller.
For example, if VIN is 5V, so SNS,OUT's MAX is 5.3V, right?
If VIN is 7.1V, so SNS,OUT's MAX is still 7V, right?
Thanks!
-Wenhao