Part Number: TPS65313-Q1
Other Parts Discussed in Thread: TPS65381A-Q1
Dear team,
My customer consider using TPS65313-Q1 PMIC for TMS570LS4357. Originally, their first option was TPS65381A-Q1 but due to current capacity of 1.2V core, they want to change to TPS65313-Q1.
The status of TPS65313-Q1 is active but sample is only available prototype at Ti.com. Is this device is not RTM status or custom device for specific customer?
Can I promote TPS65313-Q1 for my customer? If yes, How can I order sample not prototype? please let me know your opinion.
If TPS65313-Q1 is custom device for specific customer, please recommend proper PMIC for TMS570LS4357. The required specification are as follow
- input : 24V
- output : 5V/0.3A, 3.3V/0.3A , 1.2V /1A
Please review above comment and let me know your opinion.
Thank you.