Tool/software: WEBENCH® Design Tools
Hello
I need to design a boost converter using TPS61087 that provides 18.5V 250mA from a battery that may have voltage about 2.7V under load. According to TPS61087 datasheet Figure 1 and Figure 2 (Maximum Load Current vs Input Voltage for 650kHz and 1.2MHz) it is possible with fsw=650kHz.
I tried to use webench design tool to calculate the design but it doesn't accept the input parameters (I must lower output current or voltage or increase input voltage). Is that only limitation of the tool that it limits input parameters using worst case (1.2MHz) duty cycle limit? Is is safe to design the converter working at 650kHz (without webench), or I miss something?