Other Parts Discussed in Thread: BQ25895
Hi, I would like to use 2x LM74700 to protect 2x 18650 LiPo batteries against reverse polarity. The batteries are removable and there is a chance of wrong insertion in the battery holder.
The outputs of the LM74700 are or-wired as I need the capacity of both batteries in parallel.
If one or both batteries are inserted backwards then I would expect one or both LM74700 to be switched off. Is output or-ing causing any potential problems if one of the batteries is inserted backwards while the other is in the correct position?
Since the batteries are rechargeable, I need to accept reverse current, but the reverse current should be "enabled" only if a battery is connected with the proper polarity, and hence the related MOSET is on. Would this work as expected?
Best regards,
Gabriele