Hi,
I have designed a LiFePO4 battery charger based on the BQ24650.
The source power of the BQ24650 is a solar panel as this is its main purpose.
The battery spec is: 5 cells pack (approximately 17V nominal and 18V max) with a capacity of 12AH.
The solar panel is a 100W panel with an open-circuit voltage of 28 volts and 24V with load with about 4.16Amps.
To measure the actual power of the panel with load, I connected it to a power resistor of 7.3 Ohms. The voltage drop on it was 23.5V and the current through it was 3.22A so total power of about 75W.
I disconnected the resistor and connected the panel to the BQ24650.
I have two board designs that differ from one another only in their MPPT voltage - one is set to 19.9V and the other to 21.7V.
I measured the voltage and current on both designs and got these results:
First board: V=19.9, I=3.2A, P=63W --> Vbat = 17V, Ibat_charge = 3.46A, P=59W
Second board: V=21.7, I=2.9A, P=63W --> Vbat = 17V, Ibat_charge = 3.65A, P=62W
I have several questions:
1. The most important question from my side is why the used power was dropped to 63W when the solar panel can clearly produce 75W in these conditions.
2. (less important than the first question) Why there is a difference in the current produced to the battery between the two boards.
3. General question, if the solar panel introduces voltage lower than the MPPT voltage, the charge will stop, right?
See the attached schematic.
Any help is appreciated - this product is about to be manufactured and we need to resolve this quickly.
Thanks in advance,
Tomer