This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Original question:
TPS7A78: Pin to Pin Open/Short test/ External components Open/Short test
Replies: 1
Views: 92
Part Number: TPS7A78
Hello
My customer is evaluating TPS7A78EVM now. They have a question.
Could you please support the following question?
Customer comment is below,
We do a slow-down test on TPS7A78EVM (Half-bridge mode) and can't understand a waveform under slow-down mode.So we need an explanation from IC designer.
Test conditionSlow down conditon: 100V/0.5sStart voltage: AC100Vloading conditions: 390Ω
What we are concerned about is why the LDO output voltage can be recovered under slow-down mode?
Thanks
Muk
Hi Mukono-san,
I would need to see what is happening at SCIN and LDO_IN to be sure, but as the AC voltage falls the high voltage capacitor can no longer supply the full load current. If this happens, SCIN and LDO_IN will fall resulting in the output shutting down. Now that there is no load, LDO_IN will charge back up and once again turn on the LDO output.
If this is happening, increasing the capacitance in SCIN should prevent this by providing additional hold-up energy.
This is just a guess with seeing more detail. Can you supply wave-forms showing SCIN and LDO_IN when this is happening?
John Cummings 蔣康明Texas Instruments 德洲儀器Johncummings@ti.com
Please click the "Resolved" link at the bottom of this post if I have answered your question.
Thank you,