Dear Team,
Do you have further comments for this design?
BR
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kevin,
Other then the questions/comments I listed below, everything else looks okay:
Regards,
Jimmy
1.Change R31 from NC to 715 ohm + 30 ohm (add one resistor)
2.Change resistance combination to be close 3.05Kohm for 1Kohm + 1Kohm + 523ohm + 523ohm (3.046Kohm)
3.It’s original design by customer on 1.0v, I think its’ function should be discharge resistor.
4.In addition, Is IHN voltage a 4.7v and high enable?
Hi Kevin,
This clears up a few of my concerns with the schematic. Sounds like the application will be at 650kHz which is the maximum switching frequency that will enable 0.88V output rail.
The INH pin is high enable that requires a minimum of 1.8V to be above the INH high voltage threshold if the INH feature is desired. Otherwise, the INH pin may be left floating and the internal pull up source will automatically enable the part.
Regards,
Jimmy