Other Parts Discussed in Thread: LM3880,
I am using three TPSM831D31s in my design along with a LM3880MFE-1AE/NOPB. FLAG1 output from the LM3880 is going to the A_EN/B_EN pins of each of the TPSM831D31s. I am talking A_EN & B_EN from one PMBus connector (pins 7 & 4) and tying them together along with a couple of other signals through a AND gate (SN74LVC1G08DCKR) which the output goes to the EN pin of the LM3880. I have the PMBus A_EN/B_EN tied high to +3.3V via a 10K. When I plug in the PMBus it pulls the EN signal low and if I toggle the control signals in the Fusion Digital Power GUI the enable path does change. I did verify the enable signal path works by programming the supplies and then removing the PMBus. My control signal then when high & all TSPM831D31s came up. I have a couple of questions: 1) Can A_EN & B_EN pins on the PMBus be connected together? 2) Do I need to change the 10k pull-up to a different value?