Other Parts Discussed in Thread: TIDA-00318,
I am trying to wirelessly charge a 25mAh battery (~12.5mA charge current) using the BQ51050B since it's nicely integrated. However, I'm not sure whether or not the charger is able to properly control the extremely low charging currents required - lowering the charging current and disabling the termination seems to look odd below 300mA. Is there a way to configure the chip to control such currents or would it be better to use a design like the TIDA-00318 (and is that the best reference design to use or is there a more recent one?)
Ethan