Other Parts Discussed in Thread: BQ24072, BQ25120A, BQ25155
Hello,
We’re using the bq24074 to manage a Li-Ion battery pack which incorporates a 10KΩ NTC, B25/85= 3435.
Charging temperature for the battery cell is 0~45℃. This seems to be a somewhat standard charging limitation on most Li-Ion cells.
From the bq2407x datasheet:
“The bq2407x features an external battery pack temperature monitoring input. The TS input connects to the NTC thermistor in the battery pack to monitor battery temperature and prevent dangerous over-temperature conditions. “
However, we’ve just noticed that the BQ24074 default high temperature cut-off for charging is 50degC, not 45degC and the chip design doesn’t allow for this threshold to be reduced (only extended).
We did see on another thread related to the bq24072 that the bq24072 has been changed to a bq24072T to accommodate the change in cut off temperature. Unfortunately we see no such part substitute for the bq24074.
Is there any solution to reduce the upper cut off temperature of the bq24074?
Thanks in advance for your help.