Part Number: LMR16006
I'm using LMR16006. Input is around 19V, output 8.2V, 105mA. There is a divider at the SHDN pin to turn the unit off when input hits 14.5V (100K/8.8K).
I'd like to know if there is a way to slow down the turn-on a little bit? The datasheet states that it employs a soft start internally, but is there a manner to simply set up an on-delay as well?
Thanks
James