This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi William,
thanks for your questions.
Could you please confirm my understanding below:
You have two questions:
1) How to set Vout to 0.6V as the chip which is supplied by TPS62363 is damaged at higher input voltages and
2) If reflowing all chips together in mass production will have an impact on the soldering?
For 1)
I think you are referring to the Vout presets which can be selected through pins VSEL1 and VSEL0, correct? Please notice that you can also configure other (lower) voltage levels through the integrated I2C interface which is operable when VDD and AVIN are present, independent of the state of the EN pin, see section "Enabling and disabling the device" section of the device datasheet.
2) Is this an independent question? Please help me understand.
Please let me know whether my understanding was correct and provide further information on 2).
Thanks and best regards,
Britta
Hi William,
did my post answer your question or can I further assist you on this topic?
Please let me know if there is anything I can help you with or otherwise I will go ahead and close this thread.
Thanks and best regards,
Britta