Other Parts Discussed in Thread: OPA2188, , TPS54331
Attachments are problem documents, schematics and PCBs.Looking forward to hearing from you!4571.Question.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Attachments are problem documents, schematics and PCBs.Looking forward to hearing from you!4571.Question.pdf
Hi,
I have notified our expert regarding this topic. Please expect a response by 9/9/19.
Thanks,
Shinya
Now i find when i remove F26,F25,which is supply to 7 OPA2188,the buzzing disappears.WHY?
I have modified a lot of parameters, but it won't work. Only when F26 and F25 are removed, there is no noise.why
Hello,
You have a high conversion ratio assuming VCC input supply to TPS65131 is 3.3V and its output are +15V and -15V. In addition you have seven OPA2188 circuits connected to these supplies so load current will be significant. Can you tell what is load current of each OPA2188 on +15V and -15V supplies? I have a feeling that because of high conversion ratio and high load current, TPS65131 switches may be hitting current limit which is 1800mA for both boost and inverting converter (see datasheet). Another specification to check is saturation current for L2 and L3. Because switch current is high due to high conversions ration, the inductor may be getting saturated.
Kind Regards,
Liaqat
I have tested it. When I disconnect the beads F25 and F26 (the two beads are used to power the OPA2188), the ±15V load is applied directly to the 7-channel OPA2188 with a ±15V regulator. The current is only about 7 mA. Then, when the beads F25 and F26 are disconnected, I directly connect the 2.35K resistor in the ±15V output of the TPS65131, that is, the load of 6~7mA, the inductor starts. Howl.
And the input of TPS54331 and TPS65131 are 5V power supply, my power supply design is 5V to 3.3V, 5V to ±15V.The inductance is 4.7uH, how can such a small load current be saturated?
I changed the corresponding resistor divider (R57~R60) resistor value and C63 and C66 capacitor value according to the TPS65131 output voltage ±10V setting in the chip datasheet, and tried to remove the input transistor Q1, 2,3 pins directly Short circuit, the No. 1 pin is suspended (that is, the 7th pin of the TPS65131 is suspended), all tried, but it is not OK.
I need your help!
I did not know what that the load was in your application and that is why I wanted to check with you but I agree that with 7mA load, there should not be any issue with switch current limit or inductor saturation even at high conversion ratio of 15V/5V. I have reviewed rest of your design and don't see a reason for why the inductor should be buzzing. I am thinking that there may be some mechanical vibration in this particular inductor causing buzzing noise so the only thing I can suggest is to try a different inductor. The one we use in TI EVM design is Coilcraft part number XAL4030-472MEB.
Kind Regards,
Liaqat