This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 4
Views: 131
Part Number: TPS51116
Hi,
Have a question regarding the designing of TPS51116 for 1.35V DDR3L application,
I copied the circuit from the datasheet and reconfigure the output for 1.35V/0.675V DDR3L application, noticed that the PWM ON/OFF time is not consistent. What can I tweak to stabilize it.
Thanks,
SB
Hi SB,
TPS51116 is DCAP mode (constant on mode) controller.
The PWM off time may vary.
Can you double check if PWM ON time is consistent?
It will be good if you can provide PWM waveform.
Thanks
Qian
In reply to Qian Chen:
Hi Qian,
You are correct the OFF time varies, is this the D-CAP functioning as it is suppose to?
I was expecting the ON/OFF time to be consistent like my other DC-DC circuits which uses separate controllers and power FETs.
In reply to TAN SB:
Looks like the part is in discontinuous mode because at no load or light load condition.
It should be fine that off time varies.
Thanks Qian.