This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

LMZM33603: About efficiency curve data

Guru 17425 points

Replies: 4

Views: 83

Part Number: LMZM33603

Hi,

Could you tell me about efficiency curve data Fig1 ?
Is this data in forced PWM mode?

If the data includes pulse skip,
Do you have efficiency data for fixed frequency mode using the sync pin?



Best Regards,
Yusuke

  • Hi Tsukui,

    The eff curve is for force PWM mode. 

  • In reply to Andy Chen:

    Hi Yusuke-san,

    As Andy as pointed out, the eff curve is for FPWM mode. I wouldn't expect the efficiency behavior to change whether it is through RT mode or SYNC mode. As long as the external frequency is stable an fixed, I would expect similar performance for fixed frequency at RT mode and SYNC mode.

    Regards,

    Jimmy

  • In reply to Jimmy Hua:

    Jimmy-san,

    Thank you for your kind support.
    Please let me ask one more question.

    Does this device have PFM mode?
    If you have PFM mode,
    Do you have PFM efficiency data?

    Best Regards,
    Yusuke

  • In reply to Tsukui Yusuke:

    Hi Yusuke-san,

    The LMZM33603 power module only operates in "Active Mode" which is basically FPWM(Section 7.4.1). This is in continuous conduction mode with fixed switching frequency. There is no PFM option for the LMZM33603.

    If you are interested in evaluating a power module with PFM that can handle 3A current, you may be interested in the LMZM33606 power module. Figure 1 and Figure 2 of the LMZM33606 datasheet provides insight on what to expect from using the LMZM33606EVM in either FPWM or PFM mode.

    Regards,

    Jimmy

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.