Can the Sleep and Snooze mode be disabled if I don't need these functions?
If they can be disabled, how should I connect the related pins: SLEEP, SNOOZE, SNOOZE_CAP, SNOOZE_CHG ?
Thanks~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
This can be controlled by the LED_Mode pin, see below.
Unused pins are Open, float.
NOTE--Pin 45 should be connected to 3.3V.