Dear Sir/Madam,
I used the WEBENCH® POWER DESIGNER to design a DC/DC converter with the following parameters:
- Vin min = 2.7V
- Vin max = 4.5V
- Vout = 12V
- Iout = 1A
With no load and a small load like 1kohm the circuit is working good.
But when I connect a load for example 15ohm the circuit don't give the good output (10V instead of 12) and the inductor or something else is making sound.
The strange thing is that when I use no load and turn the converter on and after that connect a load of 15 ohm the converter is working fine.
What can I do to solve this problem?
I would like to thank you in advance and I am looking forward to your reply.
Regards,
Roberto