Other Parts Discussed in Thread: BQ2060, BQEVSW, EV2400
Hello All,
On the Monitor selection using the bqStudio tool - nothing shows up - is there a .bqz file for that?
Is is possible to just set up bqSudio as an SMBus monitor?
Thanks,
John W.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Onyx,
I have a large installed based of battery packs that have bq2060's installed - I need to be able to look at their EEPROM settings, etc.
Thanks,
John W.
Hi John
You can't use the bq2060 with bqstudio because it is an older device. You will need the bqEVSW provided for the device.
thanks
Onyx
Hello Onyx,
Can I get the version of bqEVSW that's on this page:
Also - on the EV2400 page - it claims:
Complete interface between the USB and SMBus, I2C (8/16) interfaces using a simple API
This implies there's an API for which to interface to the EV2400 - can you point me to that please? I haven't found any API docs for the EV2400.
Thanks,
John
Hi John,
I've reached out to Digital Marketing to fix the broken link. It should be resolved soon. If you don't see the link fixed in the next 5 days, please reach out again.
For the API, please refer to this thread: https://e2e.ti.com/support/power-management/f/196/t/773880?tisearch=e2e-sitesearch&keymatch=ev2400
Sincerely,
Bryan Kahler
Hi John,
The link is now working: http://www.ti.com/tool/BQ20Z60-R1_BQEVSW-SW
Please let me know if there are any other issues with the download.
Sincerely,
Bryan Kahler