Other Parts Discussed in Thread: LM5022
Hi E2E,
We use UCC2897A to design 2 isolated circuit and measure the VOUT ripple which is in our SPEC (+/- 5%), But the bandwidth is too slow. (< FSW/20)
Could you kindly check it and let us know that bandwidth is OK or still need to over than FSW/20?
Thanks!
1. 36~57V →12V/1.5A; FSW=250k
Transient: 0~50%
Transient: 50~100%
2. 36~57V → 54V/1A ; FSW=250K
Bandwidth:
Transient: 0~50%
Transient: 50~100%