Part Number: TPS2549
Please let me know about mean of "Internally limited" on TPS2549 Absolute maximum rating?
If there fixed current and temperature absolute maximum rating, please let me know together.
Best regards,
Satoshi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS2549
Please let me know about mean of "Internally limited" on TPS2549 Absolute maximum rating?
If there fixed current and temperature absolute maximum rating, please let me know together.
Best regards,
Satoshi
Hello Satoshi,
You can set the output current limit is variable, and can be set based on the resistance connected to ILIM_HI and ILIM_LO. Section 8.3.10 of the datasheet explains the current limit feature, as well as how to calculate the resistance to connect to each ILIM pin.
Further, you can refer to Table 2 within the datasheet to know which ILIM pin is referenced based on the mode you have the device in.
Hope this helps answer your question.
Hi Satoshi-san,
The TPS2549 has over-temperature protection so that the Junction Temperature is internally limited.
Thank you,
Eric