Other Parts Discussed in Thread: BQ76PL455A,
Hi,
I have designed PCB for BQ76PL455A according to Datasheet, Design Recommendation document and BQ76PL455A EVM and GUI user guide. After soldering all components connecting 16 cells (Samsung 25R 18650 lithium-ion) the board powered up. I had the below voltages on test points
VP = 5.29V
V5VAO = 5.29V
VDIG = 5.29V
VM = 0.3V
VREF = 0.9V
BAT16 = 46V
GND = 0V
The VM voltage ideally should be -5V whereas VREF should be 2.5V. These voltages are generated internally by the IC so there is nothing I can do. Need help getting further. Also when I try connecting the board with my laptop (USB to Serial FTDI converter), the software reports error message "could not open COM5 port".