This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Type-C/PD power chip choose

Other Parts Discussed in Thread: TPS65987D, TIDA-050012

Hi TIs

I have two designs which need to integrate Type-C/PD power function.

One is 5/9/15/20V with MAX 3A power,

The other is  5/9/15/20V with MAX 5A power,

Could you please help to advice a power chip for me?

Thanks