This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9240: PMBUS FREQUENCY_SWITCH NACK

Part Number: UCD9240

I am sending I2C commands to a UCD9240 from an FPGA on the Xilinx SP605 board.  I can send CLEAR_FAULTS and PAGE commands OK but when I send FREQUENCY_SWITCH the response is NACK even if I request the default frequency of 500 kHz.  I have a sensitive ADC attached to the FMC and I wish to implement a spread spectrum EMI reduction scheme to constantly sweep the frequency up and down by a few kHz.  I have tried preceding the FREQUENCY_SWITCH with PAGE 0x00 and PAGE 0xFF.  Every I2C command is bracketed with START and STOP.  I have tried varying the I2C clock.  The I2C driver supports clock stretch.

Thanks in advance,

Andrew.